IMX6Q IDE and compiler tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q IDE and compiler tools

Jump to solution
2,896 Views
naveenb
Contributor II

Hi, 

We have started our design using IMX6 quad processor, we are in Hardware design stage and wanted to start software application design parallely now.

I wanted to know the IDE to be used which supports the Application, Image processing (OpenCV) and Graphical user interface (OpenGl).

It would be great if anyone reply back ASAP.

Thanks!

0 Kudos
Reply
1 Solution
2,615 Views
naveenb
Contributor II
0 Kudos
Reply
2 Replies
2,615 Views
Yuri
NXP Employee
NXP Employee

Hello,

 You may look at the following Summary Page regarding recommended software

i.MX 6 Series Software and Development Tool|NXP

  NXP Linux BSP supports QT5 (please use Linux BSP documentation for more details),

therefore it makes sense to use QT5 features and tools.

Installing and Configuring QT Creator (Ubuntu) 

Computer Vision on i.MX Processors: Building OpenCV-2.4.X for Freescale's i.MX6 BSP (Yocto) 

Qt | Cross-platform software development for embedded & desktop 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,616 Views
naveenb
Contributor II

Thanks!

0 Kudos
Reply