IMX6DL XTALI and RTC_XTALI (Clock Inputs) DC Parameters.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6DL XTALI and RTC_XTALI (Clock Inputs) DC Parameters.

ソリューションへジャンプ
1,669件の閲覧回数
takashitakahash
Contributor III

Hi community.

Our customer has below question.

Would you please teach me about XTALI and RTC_XTALI (Clock Inputs) DC Parameters.

There are Only provision supplies MHz clock from an external VIL/VIH-level provisions of XTALI and RTC_XTALI Terminal ?.

Crystal oscillator child connection is not eligible?

Because for input on probes, such as quartz, and varying load capacity, such as correct DC level measurement is difficult,.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,562件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

XTALI and RTC_XTALI (Clock Inputs) DC Parameters are given in

Table 22. XTALI and RTC_XTALI DC Parameters i.MX6SDL Datasheet (rev.5, 6/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

If crystal is connected to these pins, then levels are undefined as its value is defined

by used crystal quality.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,563件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

XTALI and RTC_XTALI (Clock Inputs) DC Parameters are given in

Table 22. XTALI and RTC_XTALI DC Parameters i.MX6SDL Datasheet (rev.5, 6/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

If crystal is connected to these pins, then levels are undefined as its value is defined

by used crystal quality.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信