IMX6DL XTALI and RTC_XTALI (Clock Inputs) DC Parameters.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DL XTALI and RTC_XTALI (Clock Inputs) DC Parameters.

Jump to solution
1,666 Views
takashitakahash
Contributor III

Hi community.

Our customer has below question.

Would you please teach me about XTALI and RTC_XTALI (Clock Inputs) DC Parameters.

There are Only provision supplies MHz clock from an external VIL/VIH-level provisions of XTALI and RTC_XTALI Terminal ?.

Crystal oscillator child connection is not eligible?

Because for input on probes, such as quartz, and varying load capacity, such as correct DC level measurement is difficult,.

Labels (1)
0 Kudos
Reply
1 Solution
1,559 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

XTALI and RTC_XTALI (Clock Inputs) DC Parameters are given in

Table 22. XTALI and RTC_XTALI DC Parameters i.MX6SDL Datasheet (rev.5, 6/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

If crystal is connected to these pins, then levels are undefined as its value is defined

by used crystal quality.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,560 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

XTALI and RTC_XTALI (Clock Inputs) DC Parameters are given in

Table 22. XTALI and RTC_XTALI DC Parameters i.MX6SDL Datasheet (rev.5, 6/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

If crystal is connected to these pins, then levels are undefined as its value is defined

by used crystal quality.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply