IMX6 winCE : system Time is running faster- winCE 2013

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 winCE : system Time is running faster- winCE 2013

2,178 Views
yogeshbsa89
Contributor II

Dear Community,

SOC: IMX6

OS : WinCE 2013

We are facing strange issue in some of our systems.

System time in winCE machines is running faster . here we are observing 1 minutes gets complete 20 to 30 seconds (this is varying in different machines).

We are testing time using GetLocalTime();  GetSystemTime();  windows API. And its output time is running faster.

Although RTC time is running ok  and also we are not syncing time from SNTP in our testing.

please suggest what could be the issue.

One work around : when we disconnect IMX6 board from our system and reconnect it then this issue gets solve.

 

0 Kudos
Reply
2 Replies

1,514 Views
kakachen82
Contributor I

Have you solved this problem yet? I might be give it a try

please email to me:  kaka@baittek.com

0 Kudos
Reply

2,162 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

One can check if correct image was used as "sabre sdb" is generic name for several boards with different processors: i.MX6Q, DL, SX. For procedure issues may be sense to contact witekio directly as nxp does not support wince on i.MX6 platform.

Witekio | Witekio contact 

 

Regards

0 Kudos
Reply