IMX6 winCE : system Time is running faster- winCE 2013

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 winCE : system Time is running faster- winCE 2013

2,176 次查看
yogeshbsa89
Contributor II

Dear Community,

SOC: IMX6

OS : WinCE 2013

We are facing strange issue in some of our systems.

System time in winCE machines is running faster . here we are observing 1 minutes gets complete 20 to 30 seconds (this is varying in different machines).

We are testing time using GetLocalTime();  GetSystemTime();  windows API. And its output time is running faster.

Although RTC time is running ok  and also we are not syncing time from SNTP in our testing.

please suggest what could be the issue.

One work around : when we disconnect IMX6 board from our system and reconnect it then this issue gets solve.

 

0 项奖励
回复
2 回复数

1,512 次查看
kakachen82
Contributor I

Have you solved this problem yet? I might be give it a try

please email to me:  kaka@baittek.com

0 项奖励
回复

2,160 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

One can check if correct image was used as "sabre sdb" is generic name for several boards with different processors: i.MX6Q, DL, SX. For procedure issues may be sense to contact witekio directly as nxp does not support wince on i.MX6 platform.

Witekio | Witekio contact 

 

Regards

0 项奖励
回复