IMX6-solo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6-solo

3,374件の閲覧回数
varunjeevangoud
Contributor I

HI ,

       I have integrated focaltech Ft5x06 Touch to imx6-solo sabresd.I'm getting i2c read error in the log.In i2cdetct command it's showing uu in 0x38 address i'm suppose to get. When i used i2cset command it says device or resource busy at that address.Please help me if any one have used this ft5x06 touch sceen.probing is happening but i2c read is not happening

タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,823件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi varun

please look at

Problems Bringing up the FT5x06 touch controller

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,823件の閲覧回数
varunjeevangoud
Contributor I

and the slave address is 0x38, how you got 0x70 as slave address??

0 件の賞賛
返信

2,823件の閲覧回数
varunjeevangoud
Contributor I

hey please find this link Integration FocalTech Capacitive touch over imx6.  at last there is a driver file,copy that into your touch driver file and add also header file (.h).you can probe successful but check i2c reading or not in the log file and also using i2cdetect command.

0 件の賞賛
返信