IMX6 solo processor used part number MCIMX6S5EVM10AC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 solo processor used part number MCIMX6S5EVM10AC

965 Views
ramesh6663
Contributor III

Following are the Question please clarify us

1.Instead of the 24MHz crystal oscillator can we use an internal clock? If we use internal clock is there any performance degrade?

2.Does this chip have a Spread Spectrum Clocking feature? Please provide us

Thanks & Regards,

Rameshkumar

Labels (1)
0 Kudos
Reply
2 Replies

889 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Please refer to Hardware Development Guide for i.MX 6. According to Table 2-7

(Oscillator and clock recommendations) two options for 24 MHz clock are available :

24 MHz oscillator or external megahertz source. There are no so called internal

options. 24MHz input must not be left floating.

http://cache.nxp.com/assets/documents/data/en/user-guides/IMX6DQ6SDLHDG.pdf

 Internal PLL2 of the i.MX6 supports Spread Spectrum.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

889 Views
ramesh6663
Contributor III

Thanks Yuri

0 Kudos
Reply