IMX6 VPU h264 encoder parameters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 VPU h264 encoder parameters

ソリューションへジャンプ
8,061件の閲覧回数
anjojohn
Contributor IV

Hi All,

I am using imx6 vpu h264 encoded video fro streaming. Resolutions range from VGA to 1080x1920p. For VGA resolution (640x480) bitrate is 512 kbps. But when motion happens the video is blurred. This can be reduced if bitrate is increased. Is it possible to get more quality  if i adjust any of the h264 encoder parameters ? 

gop-size

slice-size

intra-refresh

idr-interval

Any tuned values for these parameters

ラベル(3)
0 件の賞賛
返信
1 解決策
6,928件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

try to use higher bitrate, if still has poor performance, try to enable deblocking filter

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
6,928件の閲覧回数
anjojohn
Contributor IV

how to enable deblock filter in encoding path. i am using gstreamer-1.0

0 件の賞賛
返信
6,919件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the enclosed file, the parameter "int avc_disableDeblk" in the "EncAvcParam"

6,919件の閲覧回数
anjojohn
Contributor IV

i tried the avc_disableDeblk=1 , it did improve some but the video is having blur for motion.  I can't increase bitrate above 1Mbps, as this would stop my streaming to internet. Without the bitrate parameter set and the quant-parameter to be between 20-25 , the motion blur is gone, but the variable bitrate changes abruptly between 200 Kbps and  1200 Kbps. This much sudden burst data can't be handled with my internet connection and packets will be dropped.

0 件の賞賛
返信
6,929件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

try to use higher bitrate, if still has poor performance, try to enable deblocking filter

0 件の賞賛
返信