IMX6 VPU h264 encoder parameters

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6 VPU h264 encoder parameters

跳至解决方案
8,043 次查看
anjojohn
Contributor IV

Hi All,

I am using imx6 vpu h264 encoded video fro streaming. Resolutions range from VGA to 1080x1920p. For VGA resolution (640x480) bitrate is 512 kbps. But when motion happens the video is blurred. This can be reduced if bitrate is increased. Is it possible to get more quality  if i adjust any of the h264 encoder parameters ? 

gop-size

slice-size

intra-refresh

idr-interval

Any tuned values for these parameters

标签 (3)
0 项奖励
回复
1 解答
6,910 次查看
joanxie
NXP TechSupport
NXP TechSupport

try to use higher bitrate, if still has poor performance, try to enable deblocking filter

在原帖中查看解决方案

0 项奖励
回复
4 回复数
6,910 次查看
anjojohn
Contributor IV

how to enable deblock filter in encoding path. i am using gstreamer-1.0

0 项奖励
回复
6,901 次查看
joanxie
NXP TechSupport
NXP TechSupport

refer to the enclosed file, the parameter "int avc_disableDeblk" in the "EncAvcParam"

6,901 次查看
anjojohn
Contributor IV

i tried the avc_disableDeblk=1 , it did improve some but the video is having blur for motion.  I can't increase bitrate above 1Mbps, as this would stop my streaming to internet. Without the bitrate parameter set and the quant-parameter to be between 20-25 , the motion blur is gone, but the variable bitrate changes abruptly between 200 Kbps and  1200 Kbps. This much sudden burst data can't be handled with my internet connection and packets will be dropped.

0 项奖励
回复
6,911 次查看
joanxie
NXP TechSupport
NXP TechSupport

try to use higher bitrate, if still has poor performance, try to enable deblocking filter

0 项奖励
回复