IMX6 TFT LCD configuration problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 TFT LCD configuration problem

ソリューションへジャンプ
1,958件の閲覧回数
alleenwang
Contributor II

Hi All,

I want to config the CLAA061LA0Q on imx6dl.

But this LCD had LA, VCLK etc...。

And this LCD timing sequence had some difference ...

Horizontal Timing Sequence :

lcd1.jpg

Vertical Timing Sequence :

lcd2.jpg

I can not find any setting to set the LD and VCLK on IMX6DL.

Anyone to help me with this problem?

Thanks!!!

BR.

Alleen Wang

ラベル(4)
タグ(3)
0 件の賞賛
返信
1 解決策
1,671件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alleen

seems this is just LCD matrix which requires special controller.

I.MX6 has not these signals, so seems not possible to use this LCD.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,672件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alleen

seems this is just LCD matrix which requires special controller.

I.MX6 has not these signals, so seems not possible to use this LCD.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------