IMX6 TFT LCD configuration problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 TFT LCD configuration problem

Jump to solution
1,941 Views
alleenwang
Contributor II

Hi All,

I want to config the CLAA061LA0Q on imx6dl.

But this LCD had LA, VCLK etc...。

And this LCD timing sequence had some difference ...

Horizontal Timing Sequence :

lcd1.jpg

Vertical Timing Sequence :

lcd2.jpg

I can not find any setting to set the LD and VCLK on IMX6DL.

Anyone to help me with this problem?

Thanks!!!

BR.

Alleen Wang

Labels (4)
Tags (3)
0 Kudos
Reply
1 Solution
1,654 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alleen

seems this is just LCD matrix which requires special controller.

I.MX6 has not these signals, so seems not possible to use this LCD.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,655 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alleen

seems this is just LCD matrix which requires special controller.

I.MX6 has not these signals, so seems not possible to use this LCD.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------