IMX6 TFT LCD configuration problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6 TFT LCD configuration problem

跳至解决方案
1,939 次查看
alleenwang
Contributor II

Hi All,

I want to config the CLAA061LA0Q on imx6dl.

But this LCD had LA, VCLK etc...。

And this LCD timing sequence had some difference ...

Horizontal Timing Sequence :

lcd1.jpg

Vertical Timing Sequence :

lcd2.jpg

I can not find any setting to set the LD and VCLK on IMX6DL.

Anyone to help me with this problem?

Thanks!!!

BR.

Alleen Wang

标签 (4)
标记 (3)
0 项奖励
回复
1 解答
1,652 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alleen

seems this is just LCD matrix which requires special controller.

I.MX6 has not these signals, so seems not possible to use this LCD.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,653 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alleen

seems this is just LCD matrix which requires special controller.

I.MX6 has not these signals, so seems not possible to use this LCD.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------