IMX6 Sabre Auto SDCard Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 Sabre Auto SDCard Problem

ソリューションへジャンプ
2,950件の閲覧回数
abdullahaktay
Contributor II

Hi all,

I have an imx6 saber ai board.It is booting via SATA but it is not booting from SD card.

I follow the following tutorials.

u-boot on the i.MX6 sabre sd platform in a few commands 

Booting Linux from SATA on i.MX6Q SABRE AI. 

Switch conf for SATA

S2 pin1=>0,pin2=>1,pin3=>0,pin4=>0

Switch conf for SD

S1 pin4=>0,pin5=>1

S2 pin2=>0,pin3=>1,pin4=>0

S3 pin1=>0,pin2=>0,pin3=>1,pin4=>0

What could be the problem? Is there any idea?

Thanks.

ラベル(4)
0 件の賞賛
返信
1 解決策
2,402件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Abdullah

please try to program SD card using Demo Images from link below and sect.4.3.2
Copying the full SD card image attached Linux Guide. Use sect.4.5 How to boot
the i.MX boards for booting.
http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&appType=license&location=null&Pa...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,403件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Abdullah

please try to program SD card using Demo Images from link below and sect.4.3.2
Copying the full SD card image attached Linux Guide. Use sect.4.5 How to boot
the i.MX boards for booting.
http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&appType=license&location=null&Pa...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信