IMX6 Sabre Auto SDCard Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Sabre Auto SDCard Problem

Jump to solution
2,946 Views
abdullahaktay
Contributor II

Hi all,

I have an imx6 saber ai board.It is booting via SATA but it is not booting from SD card.

I follow the following tutorials.

u-boot on the i.MX6 sabre sd platform in a few commands 

Booting Linux from SATA on i.MX6Q SABRE AI. 

Switch conf for SATA

S2 pin1=>0,pin2=>1,pin3=>0,pin4=>0

Switch conf for SD

S1 pin4=>0,pin5=>1

S2 pin2=>0,pin3=>1,pin4=>0

S3 pin1=>0,pin2=>0,pin3=>1,pin4=>0

What could be the problem? Is there any idea?

Thanks.

0 Kudos
Reply
1 Solution
2,398 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdullah

please try to program SD card using Demo Images from link below and sect.4.3.2
Copying the full SD card image attached Linux Guide. Use sect.4.5 How to boot
the i.MX boards for booting.
http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&appType=license&location=null&Pa...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,399 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdullah

please try to program SD card using Demo Images from link below and sect.4.3.2
Copying the full SD card image attached Linux Guide. Use sect.4.5 How to boot
the i.MX boards for booting.
http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&appType=license&location=null&Pa...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply