IMX6_SABRE_AI_Board Kernel building

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6_SABRE_AI_Board Kernel building

2,317 Views
hareeshth
Contributor I

I am using IMX6_KK443_200_ANDROID sources for SABRE Automotive Infotainment(6Dual SABRE-AI board) board. I need to build kernel.

I downloaded kernel from here: linux-2.6-imx.git - Freescale i.MX Linux Tree.

I have only kernel source with me ,android file system is very large in size,i couldn't download it because of poor net connection.How i build android KK443 kernel source code in ubuntu 12.04 system  (From where i can download Toolchain ) Can any one help me  ???

Labels (4)
0 Kudos
Reply
3 Replies

2,132 Views
saurabh206
Senior Contributor III
0 Kudos
Reply

2,132 Views
hareeshth
Contributor I

Hi

Saurabh

Thanks for your reply.Now I could able to download the tool chain source . But I need arm-eabi-4.6,Is arm-eabi-4.6 tool chain is available?

0 Kudos
Reply

2,132 Views
hareeshth
Contributor I

Hi,

I got arm-eabi-4.6 tool chain ...:smileycool:

Thanks.

0 Kudos
Reply