Hello, Yamaoka !
Please use Appendix A (SDMA Scripts) of the i.MX6 Reference Manual about SDMA ROM
scripts and refer to the following about SDMA and EIM.
“imx6 SDMA and EIM bus”
https://community.freescale.com/thread/324491
“i.MX6 maximum EIM burst length and performance”
https://community.freescale.com/docs/DOC-106467
As for Your questions :
1.
> Can I change SDMA burst size for EIM?
For SDMA ROM (mem-to-mem / ap_2_ap) – No.
2.
> Can I use peripheral DMA for EIM devices?
Basically – yes.
3.
> Can FPGA control SDMA access by changing a level of SDMA_EXT_EVENT after SDMA is triggerd?
Please use
“imx6 SDMA and EIM bus”
https://community.freescale.com/thread/324491
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------