IMX6 Linux Kernel console output over boot logo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 Linux Kernel console output over boot logo

4,088件の閲覧回数
subver
Contributor I

Hi. I need help to solve my problem - i've configured boot logo display during kernel boot, but kernel still prints console output over logo and login prompt. My console configured to ttymxc0 in u-boot.

If i disable framebuffer console in kernel, boot logo don't show.

How can i fix it? Thank you.

ラベル(5)
0 件の賞賛
返信
3 返答(返信)

3,452件の閲覧回数
jpdoyon
Contributor I

Look here for the proper solution (the one that worked for me).

I wound up adding the following file and directory /lib/systemd/system/[email protected]/noclear.conf

with the content of the noclear.conf:

[Service]
TTYVTDisallocate=no
0 件の賞賛
返信

4,008件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

https://community.nxp.com/docs/DOC-98109 will do some help for you.

0 件の賞賛
返信

4,008件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which i.MX6 series are you using and which version BSP are you using?

0 件の賞賛
返信