To enable RPmsg in M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

To enable RPmsg in M4

2,594 Views
subhash_ponnusamy
Contributor II

Hi,

Currently I'm working in a project where I need to send the sensor data from M4 core to A53 core in i.MX 8M Mini EVKB board using RPmsg .The available SDK's are using freeRTOS. But I need to develop in bare metal. can anyone guide me

ps. Need to implement in a project ASAP.

Regards,

Subhash

0 Kudos
Reply
3 Replies

2,557 Views
subhash_ponnusamy
Contributor II

Thanks for the response 

0 Kudos
Reply

2,588 Views
igorpadykov
NXP Employee
NXP Employee

Hi Subhash

 

one can look at rpmsg tutorial and other examples on

https://nxpmicro.github.io/rpmsg-lite/

Keil RPMSG_TTY_RTX_M4 project NXP i.MX7 SABRE board.
www.keil.com/appnotes/files/apnt_290.pdf

 

Best regards
igor

0 Kudos
Reply

2,547 Views
subhash_ponnusamy
Contributor II

Hi Igor,

      Can you please tell me where can I get  rpmsg_env_bm.c file. Because I'm using bare-metal environment. I can't able to find it .

 

Regards,

Subhash

0 Kudos
Reply