IMX6 IPU Display Clock Configuration Help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 IPU Display Clock Configuration Help

3,022件の閲覧回数
tengri
Contributor IV

Hi All,

I am having a trouble setting up the the clock rate of IPU1DI0 of IMX6Q. The platform is Nitrogen6_max fron BD and using the kernel version 3.14.52 with ubuntu trusty. Currently the parent clock of IPU1DI0 is set to PLL5_vid_dev (76MHz), and the clock divider being 2 (38MHz) according to clock summary result. I want to bring this IPU clock rate to a lower value, by increasing the clock divider. I am aware that the relevant value should be written to CCM_CHSCCDR (base+0x34) as per IMX6QRM, but where do I need to make the changes (in U-boot or kernel and what are the source files) ?

There is this parent clock assignment line in clk-imx6q.c :
clk[IMX6QDL_CLK_IPU1_DI0_PRE] = imx_clk_divider(“ipu1_di0_pre”, “ipu1_di0_pre_sel”, base + 0x34, 3, 3);

 

If I'm not mistaken, the imx_clk_divider should return the divider value. But here how the divisor is determined ? 

Thanks in Advance

ラベル(2)
0 件の賞賛
返信
1 返信

2,065件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anuradha

PLL5 selections can be found in

linux/include/dt-bindings/clock/imx6qdl-clock.h

also please refer to generic linux clock api description in

Linux/drivers/clk/clk-divider.c - Linux Cross Reference - Free Electrons 

http://elinux.org/images/b/b8/Elc2013_Clement.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信