IMX6 CSI Test Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,311件の閲覧回数
joanvicient
Contributor II

Hi all,

I am trying to enable the IPU CSI TEST_GEN_MODE. I am following the indications of the i.IMX BSP Porting Guide (Section "Configuring the CSI unit in test mode") but without succes, as I am not able to receive any image. In the document talks about a sample driver named ipuv3_csi0_chess.c. Is this code (or any equivalent) available?

Thanks

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,047件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi joan

one can try attached patch.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,048件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi joan

one can try attached patch.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,047件の閲覧回数
joanvicient
Contributor II

Thanks. The code worked!

0 件の賞賛
返信