IMX53 reset question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX53 reset question

跳至解决方案
1,710 次查看
sherry_zahid
Contributor III

Hi,

I have 2 question regarding the reset operation of the IMX53. In the datasheet on page 150, there are stated config values (e.g. 100 KΩ PU) for all the pins in "out of reset condition". Do these config values take effect when reset is applied, or after reset is released? Also, are all the internal pull ups and pull downs (described in table 112, pg. 150 of datasheet) active on device reset as well as device startup? Thanks

Kind regards,

标签 (1)
0 项奖励
回复
1 解答
1,600 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

config values take effect when reset is applied and after reset is released,

if not described separately.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,601 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

config values take effect when reset is applied and after reset is released,

if not described separately.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复