IMX53 reset question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,708件の閲覧回数
sherry_zahid
Contributor III

Hi,

I have 2 question regarding the reset operation of the IMX53. In the datasheet on page 150, there are stated config values (e.g. 100 KΩ PU) for all the pins in "out of reset condition". Do these config values take effect when reset is applied, or after reset is released? Also, are all the internal pull ups and pull downs (described in table 112, pg. 150 of datasheet) active on device reset as well as device startup? Thanks

Kind regards,

ラベル(1)
0 件の賞賛
返信
1 解決策
1,598件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

config values take effect when reset is applied and after reset is released,

if not described separately.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,599件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

config values take effect when reset is applied and after reset is released,

if not described separately.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信