IMX53 reset question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX53 reset question

Jump to solution
1,701 Views
sherry_zahid
Contributor III

Hi,

I have 2 question regarding the reset operation of the IMX53. In the datasheet on page 150, there are stated config values (e.g. 100 KΩ PU) for all the pins in "out of reset condition". Do these config values take effect when reset is applied, or after reset is released? Also, are all the internal pull ups and pull downs (described in table 112, pg. 150 of datasheet) active on device reset as well as device startup? Thanks

Kind regards,

Labels (1)
0 Kudos
Reply
1 Solution
1,591 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

config values take effect when reset is applied and after reset is released,

if not described separately.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,592 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

config values take effect when reset is applied and after reset is released,

if not described separately.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply