IMX53 QSB simple GUI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX53 QSB simple GUI

2,184件の閲覧回数
didier1
Contributor I

Hi

I need how to build a yocto image like core-image-minimal or core-image-sato but with just a simple GUI, without windows manager on a imx53 board.

Someone could give some indication?

Regards

Seize

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

1,990件の閲覧回数
didier1
Contributor I

thx igor

But i have no problem to generate image like core-image-minimal or core-image-sati.

I'd like to use one of this with a minimal graphic use interface, just create and display a picture with graphic and text.

Regars

Seize

0 件の賞賛
返信

1,990件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

H seize

latest official gui bsp is ltib, no yocto releases are provided.

Suggest also post on meta-fsl-arm mailing list

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

0 件の賞賛
返信

1,990件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

H seize

please look at

core-image-minimal Yocto for imx53qsb

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信