IMX515: media player issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX515: media player issue

2,521件の閲覧回数
ryang
Contributor III

we met imx515 WINCE Media player issue ,multimedia version is 11.04 .

question 1: when met Video decoding error, the Player programs has not responding,

>>> FSLVPUDshow:  Decodesample failed hr=80004005

>>> FSLVPUDshow: Error in Receive

PostFailureMsgToUser 1 failed 0x80004005

failed at m_pVPUDecoder->QueryVPUStatus(); in FSLVPUDshow::StopStreaming() ;

question 2: when video play to the end, the program can not automatically jump the next video:

to the end>>> FSLVPUDshow: OnEOS,

but app can not get the EC_COMPLETE,

below is VPU information:

     VPU Firmware Version =>  product: MX51 f00a | version: 0001.0004.00000028

     MPEG4PARSER_06.04.05_WINCE  build on Sep 30 2011 15:10:05

ラベル(3)
0 件の賞賛
返信
5 返答(返信)

2,076件の閲覧回数
YixingKong
Senior Contributor IV

Rita

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

2,076件の閲覧回数
YixingKong
Senior Contributor IV

Rita

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信

2,076件の閲覧回数
pawel
Contributor II

We have the same issue when we try to play a H264 stream. Same thing on FSL board and ours.

0 件の賞賛
返信

2,076件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what boards do you use? customized board or FSL board?

0 件の賞賛
返信

2,076件の閲覧回数
ryang
Contributor III

customized board

0 件の賞賛
返信