IMX DUAL Lite and IS43TR16256A-125kbl

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX DUAL Lite and IS43TR16256A-125kbl

663件の閲覧回数
kbtess
Contributor II

Hi All,

We are developing a custom board using
IMX Dual Lite processor.

We are trying to use I GB (IS43TR16256A-
125KBL) memory.

But some of the the board fails
randomly  , even if I updated the MMDC
register after running the DDR stress test tool (2.52)

, Anybody succeeded in interfacing IS43TR16256A-
125KBL with Dual lite or any other processors ?

ラベル(7)
タグ(1)
0 件の賞賛
返信
1 返信

473件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi binuthomas

DDR stress test tool does not stress all power supplies, for example

VDD_SOC_CAP, VDD_PU_CAP, as for example linux hd video

application. So one can check these and other power supplies with

oscilloscope.

One can try the following experiments to determine if it is a hardware

PCB issue. Hand solder 22uF capacitors directly under center of chip.

Solder on top of the 0402 chips.

Have software Increase voltages of ARM_CAP, SOC_CAP, PU_CAP.

Other test may be cooling/heating device - if this helps, that may point

to incorrect driver strength settings.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信