Hi All,
We are developing a custom board using
IMX Dual Lite processor.
We are trying to use I GB (IS43TR16256A-
125KBL) memory.
But some of the the board fails
randomly , even if I updated the MMDC
register after running the DDR stress test tool (2.52)
, Anybody succeeded in interfacing IS43TR16256A-
125KBL with Dual lite or any other processors ?
Hi binuthomas
DDR stress test tool does not stress all power supplies, for example
VDD_SOC_CAP, VDD_PU_CAP, as for example linux hd video
application. So one can check these and other power supplies with
oscilloscope.
One can try the following experiments to determine if it is a hardware
PCB issue. Hand solder 22uF capacitors directly under center of chip.
Solder on top of the 0402 chips.
Have software Increase voltages of ARM_CAP, SOC_CAP, PU_CAP.
Other test may be cooling/heating device - if this helps, that may point
to incorrect driver strength settings.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------