IMX 6S development set up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX 6S development set up

1,898件の閲覧回数
avenkatramani
Contributor III

Hi team,

please guide me because i am new to this linux environment.

I want to use the IMX6S, please provide some documents how to build and compile the board and some links for the initial setup of Uboot, kernel and rootfs builds for the particular IMX6.

Thanks in advice.

AK 

0 件の賞賛
返信
2 返答(返信)

1,820件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Arunkumar V,

My recommendation is downloading the Linux Document Bundle for the Kernel BSP in which you are interested.

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

For example, for the 4.1.15_2.0.0 Linux BSP Release it would be the following link (you may need to login to download this documentation bundle).

https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS

Inside you will find the i.MX Yocto Project User’s Guide. Please follow this document for instructions on how to build a Linux image for the i.MX6 NXP’s Boards. The i.MX BSPs use Yocto as a means of distribution and customization.

If you are using a third-party board some are supported by the Community BSP (link below).

http://freescale.github.io/

I hope this information helps!

Regards,

0 件の賞賛
返信

1,820件の閲覧回数
avenkatramani
Contributor III

Thanks for the replay.

I checked the links and really helpful.

is it possible to compile the Uboot, kernel (latest/new) alone with the custom rootfs?

can you share some documents/links for the imx6s kernel details and build set up.

Thanks in advice.

 AK 

0 件の賞賛
返信