Error occurs when bitbake fsl-image-qt5 on Ubuntu 16.04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error occurs when bitbake fsl-image-qt5 on Ubuntu 16.04

Jump to solution
1,661 Views
wangtsungli
Contributor IV

Hi Community,

I'm using yocto 2.4 to build rootfs.

I had install the essential package that mentioned in i.MX Yocto Project User's Guide.

But when I execute bitbake fsl-image-qt5, I would get a warning like below.

WARNING: Host distribution "Ubuntu-16.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.

Then compile will keep running until I met a new error like below.

| make[4]: Leaving directory `/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/git/nptl'
| make[3]: Leaving directory `/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/git/elf'
| arm-poky-linux-gnueabi-gcc -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 --sysroot=/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/sysroots/imx6qsabresd-tcbootstrap -shared -static-libgcc -Wl,-O1 -Wl,-z,defs -Wl,-dynamic-linker=/lib/ld-linux-armhf.so.3 -B/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/csu/ -Wl,--version-script=/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/libc.map -Wl,-soname=libc.so.6 -Wl,-z,combreloc -Wl,-z,relro -Wl,--hash-style=both -nostdlib -nostartfiles -e __libc_main -L/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi -L/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/math -L/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/elf -L/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/dlfcn -L/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/nss -L/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/nis -L/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/rt -L/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/resolv -L/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/crypt -L/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/mathvec -L/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/nptl -Wl,-rpath-link=/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi:/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/math:/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/elf:/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/dlfcn:/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/nss:/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/nis:/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/rt:/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/resolv:/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/crypt:/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/mathvec:/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/nptl -o /mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/libc.so -T /mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/shlib.lds /mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/csu/abi-note.o /mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/elf/soinit.os /mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/libc_pic.os /mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/elf/sofini.os /mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/elf/interp.os /mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/elf/ld.so -lgcc
| /mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/sysroots/x86_64-linux/usr/libexec/arm-poky-linux-gnueabi.gcc-cross-initial-arm/gcc/arm-poky-linux-gnueabi/6.2.0/ld:/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/shlib.lds:156: syntax error
| collect2: error: ld returned 1 exit status
| make[2]: *** [/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/build-arm-poky-linux-gnueabi/libc.so] Error 1
| make[2]: Leaving directory `/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/git/elf'
| make[1]: *** [elf/subdir_lib] Error 2
| make[1]: Leaving directory `/mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/git'
| ERROR: oe_runmake failed
| make: *** [all] Error 2
| ERROR: Function failed: do_compile (log file is located at /mnt/raid121/victor/yocto2.4/build-wayland-q/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.24-r0/temp/log.do_compile.5975)
ERROR: Task (/mnt/raid121/victor/yocto2.4/sources/poky/meta/recipes-core/glibc/glibc_2.24.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2902 tasks of which 2899 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/mnt/raid121/victor/yocto2.4/sources/poky/meta/recipes-core/glibc/glibc_2.24.bb:do_compile
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

I think the main cause is "shlib.lds:156: syntax error".

Did I miss anything?

How to fix this error?

Thanks in Advanced!

0 Kudos
Reply
1 Solution
1,173 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi tsung,

This look like you have to install a package that is not there such as glib or binutils, I strongly recommend to unnistall yocto and reinstall again.

Regards

View solution in original post

0 Kudos
Reply
2 Replies
1,174 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi tsung,

This look like you have to install a package that is not there such as glib or binutils, I strongly recommend to unnistall yocto and reinstall again.

Regards

0 Kudos
Reply
1,173 Views
wangtsungli
Contributor IV

Thanks for your help.

After I reinstall Yocto Project, it's solved my problem!

0 Kudos
Reply