I2D Devices Not detecting...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2D Devices Not detecting...

1,373 Views
priyangeorge
Contributor I

Hi everyone,

I am using I.MX257 processor. I have connected some devices to i2c bus 2. When i probe the i2c 2 line from linux terminal the devices are not showing up. But when connecting a CRO probe accros SDA line & ground and probing the I2C lines from linux terminal the device are showing up. I dont know what is the reason behind this. Can anyone help me with this.

Labels (1)
0 Kudos
Reply
1 Reply

1,280 Views
igorpadykov
NXP Employee
NXP Employee

Hi priyan

this may be bad contact or absence of pull-up resistor, please check it.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply