I2C test application from userspace

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I2C test application from userspace

跳至解决方案
22,060 次查看
srinivasanshanm
Contributor III

Dear All,


I'm trying to write the eeprom userspace test application,


when I run the below test app, I see the below messages

BusyBox v1.15.0 () built-in shell (ash)

Enter 'help' for a list of built-in commands.

root@freescale ~$ MY_TEST_APPLICATION_EEPROM

SUCCESS: open(3) passed

ERROR: ioctl(fd, I2C_SLAVE, 0x50) failed

root@freescale ~$

I even tried changing it to   "status = ioctl(fd, I2C_SLAVE_FORCE, i2c_addr);"  , but still the same issue, could you please let me know how to get rid of this issue, as am trying this from since 2 days, not able to succeed further

Any help would be greatly appreciated

Thanks in advance,

#include <stdio.h>

#include <unistd.h>

#include <stdlib.h>

#include <sys/types.h>

#include <sys/stat.h>

#include <sys/ioctl.h>

#include <fcntl.h>

#include <linux/fs.h>

#include <errno.h>

#include <string.h>

#include <linux/i2c-dev.h>

#include <linux/i2c.h>

    /* chmod 666 /dev/i2c-0 */

int main(void)

{

       // Data to be written to eeprom

unsigned char wbuf[17] =  {   0x00, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17, 0x18, 0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E, 0x1F };                

unsigned char rbuf[16];

int i2c_addr = 0xa0;

int status;

unsigned short int i;

// OPENING I2C DEVICE

int fd = open("/dev/i2c-0", O_RDWR);

if (fd < 0) {

printf("ERROR: open(%d) failed\n", fd);

return -1;

}

  printf("\nSUCCESS: open(%d) passed\n", fd);

// SETTING EEPROM ADDR

    status = ioctl(fd, I2C_SLAVE, i2c_addr>>1);

    if (status < 0)

    {

printf("ERROR: ioctl(fd, I2C_SLAVE, 0x%02X) failed\n", i2c_addr);

close(fd);

return -1;

        }

    printf("\nSUCCESS: ioctl(fd, I2C_SLAVE, 0x%02X>>1) passed\n", i2c_addr);

// WRITING TO EEPROM

printf ("\nPerforming EEPROM Write operation\n");

write(fd,wbuf,16);

sleep(10); //till eeprom completes writes

if (write(fd,wbuf,16) != 16) {

printf("ERROR: write() failed\n");

close(fd);

return -1;

}

printf("\nSUCCESS: Data written to the EEPROM\n");

// READING FROM EEPROM

printf ("\nPerforming EEPROM Read operation\n");

wbuf[0]=0;

if(write(fd,wbuf,1)!=1){

printf("ERROR: buffer pointer initialization of read() failed\n");

}

  if (read(fd,rbuf,16) != 16) {

printf("ERROR: read() failed\n");

close(fd);

return -1;

}

for(i = 0; i< 16; i++)

printf("ReadBuffer[%d] %d \r\n", i, rbuf[i]);

printf("\nSUCCESS: Data READ from the EEPROM\n");

printf("\neerprom test successfull \n");

close(fd);

}

标签 (2)
0 项奖励
回复
1 解答
6,597 次查看
raymondwang
Senior Contributor I

You can refer to http://www.lm-sensors.org/browser/i2c-tools/trunk/eepromer?rev=5202

There are some examples of i2c utilities to access EEPROM (also including 24Cxx serial eeprom).

在原帖中查看解决方案

0 项奖励
回复
7 回复数
6,597 次查看
YixingKong
Senior Contributor IV

Srinivasan

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel

free to contact Freescale.

Thanks,
Yixing

0 项奖励
回复
6,597 次查看
srinivasanshanm
Contributor III

Please close this issue it is resolved, thanks a lot for your support

0 项奖励
回复
6,598 次查看
raymondwang
Senior Contributor I

You can refer to http://www.lm-sensors.org/browser/i2c-tools/trunk/eepromer?rev=5202

There are some examples of i2c utilities to access EEPROM (also including 24Cxx serial eeprom).

0 项奖励
回复
6,597 次查看
srinivasanshanm
Contributor III

Could anybody please do the needful in addressing the above thread, as early as possible,

Any help would be greatly appreciated,

Many Many thanks in advance again...

0 项奖励
回复
6,597 次查看
Raybiztech
Contributor V

Hi Srinivasan,

     There can be 3 different possibilities,

1) Each registered i2c adapter gets a number starting from 0 ,check eeprom is connected to which adaptor.  

     see /sys/class/i2c-dev/ to see what number corresponds to which adapter.

2) verify eeprom address in datasheet.

3) I think Right shift operation is not necessary as generally driver is take care of sending 7 bit device address in upper bits of byte.

If you share eeprom datasheet as well as board specification it will be better.

Regards,

sasidhar

0 项奖励
回复
6,592 次查看
srinivasanshanm
Contributor III

Hi sasidhar

Thanks a lot for your response,

Am using eeprom 24c08, whose slave address is 0x50

Please find the attached datasheet, evn I tried giving seven bit address this didnt work for me

Thanks in advance

0 项奖励
回复
6,592 次查看
Raybiztech
Contributor V

Hi Srinivasan,

      If you look into data sheet the first 4 bits of device address always be 1010 ie. 0xa while last 4 bits can be changed based on "Table 3. Device Select Code" on page no 3 of datasheet. check for chip enable pin(3) is connected to vcc or gnd ie 1 or 0. if that pin is connected to 1 then b3 bit of address should be 1 & if pin is connected to 0 then b3 bit of address should be 0.otherwise device wont response.


if chip enable pin is 1 then device address is 10101XXX

if chip enable pin is 0 then device address is 10100XXX.

Please read "write operation" on page no 7 of data sheet carefully.

also refer following link

https://www.kernel.org/doc/Documentation/i2c/dev-interface

regards,

Sasidhar

0 项奖励
回复