Hello all,
I am using sabresd with 2014.01 u-boot ("mx6qsabresd_config" configuration) and I got the u-boot prompt on the board. But there is no "i2c" command by default. And I tried to bring up the "i2c" command. For this, I added these lines in "include/configs/mx6sabresd.h" file (I referred LTIB BSP u-boot code which is 2009.08 version )
/* I2C configs */
#define CONFIG_CMD_I2C
#define CONFIG_SYS_I2C 1
#define CONFIG_I2C_MXC 1
#define CONFIG_SYS_I2C_PORT I2C2_BASE_ADDR
#define CONFIG_SYS_I2C_SPEED 100000
#define CONFIG_SYS_I2C_SLAVE 0x8
And with this settings, I got the u-boot prompt with i2c command but it is not working properly. Below is the attached boot log message:
U-Boot 2014.01 (Apr 23 2014 - 17:03:14)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: POR
Board: MX6-SabreSD
I2C: Error, wrong i2c adapter 0 max 0 possible
ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
Error, wrong i2c adapter 0 max 0 possible
Error, wrong i2c adapter 0 max 0 possible
auto-detected panel HDMI
Display: HDMI (1024x768)
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Hit any key to stop autoboot: 0
=> i2c probe
Valid chip addresses:Error, wrong i2c adapter 0 max 0 possible
Error, wrong i2c adapter 0 max 0 possible
data abort
MAYBE you should read doc/README.arm-unaligned-accesses
pc : [<4ffa0bf4>] lr : [<4ff8d220>]
sp : 4f570dd8 ip : 00000034 fp : 00000000
r10: 00000002 r9 : 4f570f30 r8 : 4f876cc8
r7 : 00000000 r6 : ffffffff r5 : 00000000 r4 : 4ffa0bd0
r3 : 00000083 r2 : 00000060 r1 : 00000000 r0 : 00000000
Flags: nZCv IRQs off FIQs off Mode SVC_32
Resetting CPU ...
resetting ...
U-Boot 2014.01 (Apr 23 2014 - 17:03:14)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: WDOG
Board: MX6-SabreSD
I2C: Error, wrong i2c adapter 0 max 0 possible
ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
Error, wrong i2c adapter 0 max 0 possible
Error, wrong i2c adapter 0 max 0 possible
auto-detected panel HDMI
Display: HDMI (1024x768)
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Hit any key to stop autoboot: 0
=>
As you can see, when I try for "i2c probe", the board is reset with "Error, wrong i2c adapter 0 max 0 possible" error message. Do I need any other configuration for "i2c" command to work properly?
Thanks in advance.
已解决! 转到解答。
 
					
				
		
 fabio_estevam
		
			fabio_estevam
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Niklas,
I have just tested with U-boot 2014.04 and the i2c commands work fine. You can apply this patch that adds pfuze100 pmic which is connected via i2c:
Hi Jai.
Did you manage to solve this problem?
I also have the same problem (right now using 2013.10).
When I tried to set something (speed) or do a probe, u-boot restarts.
U-Boot > i2c speed 100000
Setting bus speed to 100000 Hz
data abort
MAYBE you should read doc/README.arm-unaligned-accesses
pc : [<4ff9ad30>] lr : [<4ff9a75c>]
sp : 4f584e00 ip : 00000000 fp : 4f585860
r10: 4ffba700 r9 : 4f584f38 r8 : 00000003
r7 : 00000002 r6 : 4f5858a4 r5 : 4ffb983c r4 : 00000000
r3 : 00000039 r2 : 00000300 r1 : 4ffae44c r0 : 4ffae4dc
Flags: nzCv IRQs off FIQs off Mode SVC_32
Resetting CPU ...
resetting ...
Thanks,
Niklas
Hi Nilkas,
For the post I made above, I made a small mistake in adding a line in ""include/configs/mx6sabresd.h". I added " #define CONFIG_I2C_MXC " but it must be "#define CONFIG_SYS_I2C_MXC". After changing this line i2c command works but "i2c probe" does not show any devices connected to it even after probing all the buses.
But it works fine in 2014.04 u-boot with the patch posted by Fabio.[[U-Boot] [PATCH v3] mx6sabred: Add PFUZE100 PMIC support]. Please do try this.
 
					
				
		
 fabio_estevam
		
			fabio_estevam
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Niklas,
I have just tested with U-boot 2014.04 and the i2c commands work fine. You can apply this patch that adds pfuze100 pmic which is connected via i2c:
Thanks Fabio.It works fine in 2014.04 u-boot with the above patch.
And for the post I made above, I made a small mistake in adding a line in ""include/configs/mx6sabresd.h". I added " #define CONFIG_I2C_MXC " but it must be "#define CONFIG_SYS_I2C_MXC". After changing this line i2c command works but "i2c probe" does not show any devices connected to it even after probing all the buses.
Hi Fabio,
I took mx6qsabrelite in 2014.01 as reference (where i2c is working fine in sabrelite baord) and looked at it. And i guess that the error we saw in the boot log is thrown from the file "drivers/i2c/i2c_core.c", in the function "i2c_set_bus_num()", line
| max = ll_entry_count(struct i2c_adapter, i2c); if (I2C_ADAPTER(bus) >= max) { printf("Error, wrong i2c adapter %d max %d possible\n", I2C_ADAPTER(bus), max); return -2; } | |
I put some debug messages there and found that the variable "max" is set to 0 in case of sabresd, but in the case of sabrelite it is 3. This function is called from "arch/arm/lib/board.c" which is common to both sabrelite and sabresd and I guess no board specific confgiuration with respect to i2c is made before that function call. So I wonder how the "max" variable differs in these two cases. Meanwhile I googeled for "ll_entry_count" which specifies " returns the number of elements in the linker generated array" and I am not sure what is linker generated array.
And so I cannot guess what is the cause of this error. Can you guide me in this issue?
Thanks