I2C bus communication error without ACK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I2C bus communication error without ACK

2,170 次查看
vincentchou
Contributor IV

Hi! Support, 

We designed a camera sensor module based on OV7725 sensor.  We used i.MX6Q Sabresd board to develop the driver for Android 5.1.1 and Linux 3.14.52 kernel.  Unfortunately I have not been able to communicate with the sensor module.  Even though we tested OV5640 module on Sabresd board, we have not been able to use the same I2C configuration to communicate with OV7725 sensor.  I traced into the i2c-imx.c and found out there are errors generated from the following two functions: i2c_imx_trx_complete and i2c_imx_acked.  I also checked the content of I2C_I2SR and it generates 0xa1 and 0xa5 most of the time.  I suspect that OV7725 sensor does not support I2C protocol, but only SCCB protocol. 

In addition, I examine the code of i2c-imx.c.  It seems the code does not support I2C_FUNC_PROTOCOL_MANGLING,  I2C_M_IGNORE_NAK and I2C_M_NO_RD_ACK.  Could you kindly tell me how to accommodate the NO_ACK condition?  Should I change I2C driver completely? Thanks!

Vincent

0 项奖励
回复
1 回复

1,516 次查看
Pavel
NXP Employee
NXP Employee

Look at the following page:

https://community.nxp.com/thread/313467

 

This page shows that i.MX6 I2C and i.MX6 BSP can be used for camera connection using SCCB protocol.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复