I would like to run a VxWorks 7 image project using the i.MX6 Sabre development board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I would like to run a VxWorks 7 image project using the i.MX6 Sabre development board

1,086 次查看
paulsayers
Contributor I

The development board is currently using U-Boot 2015.04-00392-g6581aea-dirty (Jul 02 2016 - 14:06:02) and is booting an Android image. I have a simple VxWorks 7 VIP built using the BSP for the i.MX6 Sabre board. The SDCard is formatted for Android OS so how do I get the VxWorks image onto the SD card and how do I boot to this image instead of the Android OS?

0 项奖励
回复
1 回复

901 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi paul,

You may need contact Winriver: NXP - Partner Profile Information For that task.

Regards

0 项奖励
回复