I would like to run a VxWorks 7 image project using the i.MX6 Sabre development board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I would like to run a VxWorks 7 image project using the i.MX6 Sabre development board

1,121 Views
paulsayers
Contributor I

The development board is currently using U-Boot 2015.04-00392-g6581aea-dirty (Jul 02 2016 - 14:06:02) and is booting an Android image. I have a simple VxWorks 7 VIP built using the BSP for the i.MX6 Sabre board. The SDCard is formatted for Android OS so how do I get the VxWorks image onto the SD card and how do I boot to this image instead of the Android OS?

0 Kudos
Reply
1 Reply

936 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi paul,

You may need contact Winriver: NXP - Partner Profile Information For that task.

Regards

0 Kudos
Reply