I want to use qtquickwiget and qmediaplayer which backend and image should I build is the best

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I want to use qtquickwiget and qmediaplayer which backend and image should I build is the best

902 次查看
wangtsungli
Contributor IV

Hi community,

I had designed an application with QT5.4.

And I used Qquickwidget and Qmediaplayer to complete my functionality.

I am getting start at using Yocto Project 2.0 released by freescale.

And I wondering which backend and image is suitable for me to use.

According to the reference, it has some images that I can choose to build related to below picture.

pastedImage_1.png

I suppose that these are options which rootfs I want to build.

And below picture is the option to choose which backend that you want.

pastedImage_2.png

Here is my question.

which backend and rootfs do I need to build for running my application?

Is there any suggestions?

Additional question, can anyone teach what is the difference between wayland and X11?

Although I have a lot of research on the internet, I still cannot understand what are these two suppose to do.

And still cannot understand what is the difference between -platform wayland and -platform eglfs.

I would be grateful that anyone who can teach me.

Thanks in advanced!

0 项奖励
回复
0 回复数