I need to communicate quectel module using usb protocol rt1170 for sending receiving AT commands

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need to communicate quectel module using usb protocol rt1170 for sending receiving AT commands

1,198 Views
Bharath_S
Contributor I

I need to communicate quectel module using usb protocol using rt1170 arm processor for sending receiving AT commands response, so for this i gone through the usb example but i couldn't able to understand what are parameters i need to change for this if any one knows what are thigs i need to know before starting modifications 

0 Kudos
Reply
1 Reply

1,178 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, could you share the datasheet of the Quectel or the pinout, maybe you need to use Uart to send the AT command through RX & TX, if that is the right protocol, you can use the example from the SDK.

Best regards,
Pavel

0 Kudos
Reply