I need to communicate quectel module using usb protocol rt1170 for sending receiving AT commands

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I need to communicate quectel module using usb protocol rt1170 for sending receiving AT commands

1,219 次查看
Bharath_S
Contributor I

I need to communicate quectel module using usb protocol using rt1170 arm processor for sending receiving AT commands response, so for this i gone through the usb example but i couldn't able to understand what are parameters i need to change for this if any one knows what are thigs i need to know before starting modifications 

0 项奖励
回复
1 回复

1,199 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, could you share the datasheet of the Quectel or the pinout, maybe you need to use Uart to send the AT command through RX & TX, if that is the right protocol, you can use the example from the SDK.

Best regards,
Pavel

0 项奖励
回复