I need help with audio routing in WM8960

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I need help with audio routing in WM8960

2,820件の閲覧回数
subash_p
Contributor III

Hi, I have a custom board IMX8QXP-MEK with the integration of WM8960. By default, the RINPUT1 is connected to my main board IC. I can hear the .mp3 file sound from the WM8960, but I can't hear the audio from the radio chip. The radio chip ROUT and LOUT are connected to RINPUT2 and LINPUT2. Do I need to modify any DTS file or .c file to hear the audio?

Regards,
subash

0 件の賞賛
返信
11 返答(返信)

2,801件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

2,797件の閲覧回数
subash_p
Contributor III

Kernel version is 6.1.36

0 件の賞賛
返信

2,747件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

This is the driver of WM8960.

https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/sound/soc/codecs/wm8960.c

 

This is a document talk about the wm8960 driver. Although it is long time ago, the concept is the same.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/WM8960-audio-codec/ta-p/1119101

 

You could check the alsamixer first to see the switches/mutes are setting correct.

0 件の賞賛
返信

2,744件の閲覧回数
subash_p
Contributor III

Hi @jimmychan

I enabled all of the RINPUT2 and LINPUT2 options in Alsamixer but I can't hear any sound from my radio chip

 

Thanks,

subash.p

0 件の賞賛
返信

2,734件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Please check the WM8960 block diagram. There are different path from INPUT to OUTPUT. You could input the audio signal to the ADC. Or you could input the audio signal direct to the output bypass the ADC. Please double check which path you choose and select the correct input in the output mixer.

2,510件の閲覧回数
subash_p
Contributor III

Hi @jimmychan 

Am I need to modify wm8960 dts file ?

0 件の賞賛
返信

2,493件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

What is your wm8960 setting of routing in the dts file?

0 件の賞賛
返信

2,481件の閲覧回数
subash_p
Contributor III

Hi @jimmychan 

sof-sound-wm8960 {
compatible = "simple-audio-card";
label = "wm8960-audio";
simple-audio-card,bitclock-master = <&sndcodec>;
simple-audio-card,frame-master = <&sndcodec>;
hp-det-gpio = <&lsio_gpio1 0 0>;
mic-det-gpio = <&lsio_gpio1 0 0>;
simple-audio-card,widgets =
"Headphone", "Headphone Jack",
"Speaker", "Ext Spk",
"Microphone", "Mic Jack";
simple-audio-card,audio-routing =
"Headphone Jack", "HP_L",
"Headphone Jack", "HP_R",
"Ext Spk", "SPK_LP",
"Ext Spk", "SPK_LN",
"Ext Spk", "SPK_RP",
"Ext Spk", "SPK_RN",
"LINPUT2", "Mic Jack",
"LINPUT3", "Mic Jack",
"RINPUT1", "Mic Jack",
"RINPUT2", "Mic Jack",
"Playback", "SAI1.OUT",
"SAI1.IN", "Capture";
simple-audio-card,dai-link {
format = "i2s";
cpu {
sound-dai = <&dsp 1>;
};
sndcodec: codec {
sound-dai = <&wm8960>;
};
};
};

0 件の賞賛
返信

2,473件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Is your signal input through the mic jack? If yes, as your headphone also using the same gpio for detection, the output will be go to the headphone, not the speaker.

0 件の賞賛
返信

2,465件の閲覧回数
subash_p
Contributor III

HI @jimmychan  

On my custom board, RINPUT2 and LINPUT2 are connected to si4754 LOUT and ROUT. I'm not sure the signal is being sent through the mic jack.

0 件の賞賛
返信

2,435件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

If the RINPUT2 and LINPUT2 are connected directly to SI4754 on the circuit and not through the mic. jack, then please remove the "RINPUT2", "Mic Jack" and "LINPUT2", "Mic Jack" in the routing.

0 件の賞賛
返信