I'm not able to use Second SD port, when flashing MMC using imx28_ivt_linux.sb

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I'm not able to use Second SD port, when flashing MMC using imx28_ivt_linux.sb

1,838 次查看
swaraj
Contributor II

When kernel is loaded with imx28_ivt_linux.sb and mk_mx28_sd, i am able to login directly without U-Boot prompt but i'm not able to use SD1 (2nd SD slot).

Can anyone help me..

标签 (1)
0 项奖励
回复
3 回复数

1,590 次查看
Matt_ng9
Contributor III

Try this command line...

noinitrd console=ttyAM0,115200 root=/dev/mmcblk0p3 rw rootwait ip=none ssp1

 

Got this from page 5-24 of i.MX28_Linux_BSP_UG.pdf

0 项奖励
回复

1,590 次查看
swaraj
Contributor II

My command line is:

Kernel command line: noinitrd console=ttyAM0,115200 root=/dev/mmcblk0p3 rw rootwait ip=none gpmi

this is by default set in (2.6.35.3 kernel )

 

Other thing what i noticed is that NAND and SD1 will be sharing pins, So how should i configure them by disabling NAND pins...

 



Sinan Emre Kutlu said:
I think it depends on your kernel command line
0 项奖励
回复

1,590 次查看
snan1z
Contributor I
I think it depends on your kernel command line
0 项奖励
回复