Perhaps the problem concerns with the low available current from internal i.MX28
regulators in default (start) configuration. This may take place when external parts
(say, DDR) are fed from i.MX28 PMU.
According to app note AN4199 : “The 5-V source can be taken from a
universal serial bus (USB) connection […]. There is a 100-mA input current
limit when the system is powering up from the Power-Off state. Product designers
should pay attention to ensure the 100 mA is sufficient for the total system
consumption during cold-boot or reboot.”
For 5V only configuration, first please refer to section 4.1.2.1 (VDD5V source only: hardware
configuration) of AN4199. Please pay attention on the schematic, shown on Figure 9 (Hardware
connections for VDD5V-only applications). As for software, please use the recent official Freescale
Linux BSP on the Web. Next, according to section 4.1.2.2 (VDD5V source only: software configuration) :
"For an application that uses the VDD5V source only, NO_DCDC_BATT_SOURCE must be defined on
power_prep.c in the bootlet codes. Additionally, the programmer should ensure that
NO_VDD5V_SOURCE is not defined. For more details, see to the Linux BSP User’s Guide."
http://cache.freescale.com/files/32bit/doc/app_note/AN4199.pdf
https://www.freescale.com/webapp/Download?colCode=L2.6.35_1.1.0_ER_SOURCE&appType=license&location=n...
https://www.freescale.com/webapp/Download?colCode=L2.6.35_1.1.0_LINUX_DOCS&location=null
Summary Page :
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX285&nodeId=018rH3ZrDRA24A&fpsp=1&...