I.MX8M plus AI Robot platform Ubuntu OS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I.MX8M plus AI Robot platform Ubuntu OS

跳至解决方案
98,875 次查看
刘国华
Contributor III

@xiaodong_zhang 

  There are some questions from our customer need your commet :

  1. Does I.MX8M plus support all operator included by tensor flow lite ?   I saw some words in the i.MX_Machine_Learning_User's_Guide.pdf . The TensorFlow Lite library uses the Android NN API implementation from the GPU/NPU driver for running inference using the GPU/NPU hardware accelerator. The implemented NN API version is 1.2, which has limitations in supported tensor data types and operations, compared to the feature set of TensorFlow Lite. Therefore,
    some models may work without acceleration enabled, but may fail when using the NN API. So the answer is NOT ?                                 
  2. Right now the I.MX8M plus support Ubuntu rootfs , does it include ROS and some ML sample ? Our customer is using Jetson Nano , it is base on Ubuntu rootfs , support ROS default . Right now they are evaluating replacing the Jetson nano with I.MX8M plus , they would like to use ubuntu . 
  3. I noted the I.MX8M plus is 2.3 TOPS base on int8 , compare to the Jetson Nano 472 GFLOPS, how to understand the advantage between them ?
  4. Could you help to share some information about the camera using in the AI Robot EVK ?
标记 (1)
1 解答
98,851 次查看
xiaodong_zhang
NXP Employee
NXP Employee

According to the below picture

xiaodong_zhang_0-1622019188909.jpeg

472GFLOPS(FP16) = 472*2GOPS(INT8)=472*2%1024TOPS ≈ 0.92TOPS

在原帖中查看解决方案

0 项奖励
回复
21 回复数
97,680 次查看
刘国华
Contributor III

@xiaodong_zhang 

As right now the ubuntu20.04 rootfs is base on I.MX8M plus EVK , we are going to install the ubuntu 20.04 on the AI robot EVK , please help to share the user guide . Thanks

0 项奖励
回复
97,664 次查看
xiaodong_zhang
NXP Employee
NXP Employee

@刘国华 

Please desktop manifest as the following:

repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-gatesgarth -m imx-5.10.9-1.0.0_desktop.xml

And then, apply patch 0001-Add-to-support-i.MX8M-Plus-AI-Robot-board-and-some-t.patch for layer meta-nxp-desktop and untar meta-imx8mp-ai-robot-L5.10.9-gatesgarth.tar.gz under <Yocto folder>/source.

$ DISTRO=imx-desktop-xwayland MACHINE=imx8mpairobotdesktop source imx-setup-desktop.sh -b build-ai-robot-desktop

After the above command, you should add BBLAYERS += "${BSPDIR}/sources/meta-imx8mp-ai-robot " in <Yocto folder>/build-ai-robot-desktop/bblayers.conf
$bitbake imx-image-desktop

Note:

<Yocto folder>/source/meta-nxp-desktop/conf/distro/imx-desktop-xwayland.conf has some configure options like IMAGE_ROOTFS_SIZE, you can change it for larger size of rootfs. Default user account and password are all user.  You can change it by the below guide.

# Set user account and password
#APTGET_ADD_USER = "user:password:shell"
# format 'name:password:shell'.
# 'name' is the user name.
# 'password' is an encrypted password (e.g. generated with
# `echo "P4sSw0rD" \| openssl passwd -stdin`).
# If empty or missing, they'll get an empty password.
# 'shell' is the default shell (if empty, default is /bin/sh).

0 项奖励
回复
97,589 次查看
khang_letruong
Senior Contributor III

Dear @xiaodong_zhang ,

I'm interested in testing this AI Robot Platform but I'm struggling the following error while doing the rootfs :

Initialising tasks: 100% |############################################################| Time: 0:00:03
Sstate summary: Wanted 287 Found 285 Missed 2 Current 2317 (99% match, 99% complete)
NOTE: Executing Tasks
ERROR: imx-image-desktop-20.04.2-r0 do_rootfs: [log_check] imx-image-desktop: found 1 error message in the logfile:
[log_check] Failed to connect to bus: Host is down

ERROR: Logfile of failure stored in: /backup/NXP/Yocto/imx-yocto-bsp-5_10_9-1_0_0-desktop/build-ai-robot-desktop/tmp/work/imx8mp_ai_robot-fsl-linux/imx-image-desktop/20.04.2-r0/temp/log.do_rootfs.30696
ERROR: Task (/backup/NXP/Yocto/imx-yocto-bsp-5_10_9-1_0_0-desktop/sources/meta-nxp-desktop/recipes-fsl/images/imx-image-desktop.bb:do_rootfs) failed with exit code '1'


My host is Ubuntu-18.04. I wonder if you could help to solve this issue please ?

Thanks very in advance and best regards,
Khang

 

0 项奖励
回复
97,546 次查看
xiaodong_zhang
NXP Employee
NXP Employee

@khang_letruong 

  Please send me your error log (file log.do_rootfs.30696).

0 项奖励
回复
97,536 次查看
khang_letruong
Senior Contributor III

Hi @xiaodong_zhang ,

Please find the requested file in attachment. Additional information :I still faced this error within Ubuntu-20.04 as host.

Br,
Khang

0 项奖励
回复
97,531 次查看
xiaodong_zhang
NXP Employee
NXP Employee

@khang_letruong 

what configuration of your build server ?

BTW, here is my log:

Creating config file /etc/idmapd.conf with new version
Adding system user `statd' (UID 116) ...
Adding new user `statd' (UID 116) with group `nogroup' ...
Not creating home directory `/var/lib/nfs'.
Created symlink /etc/systemd/system/multi-user.target.wants/nfs-client.target -> /lib/systemd/system/nfs-client.target.
Created symlink /etc/systemd/system/remote-fs.target.wants/nfs-client.target -> /lib/systemd/system/nfs-client.target.
Setting up libgcc-9-dev:arm64 (9.3.0-17ubuntu1~20.04) ...
Setting up libltdl-dev:arm64 (2.4.6-14) ...
Setting up pkg-config (0.29.1-0ubuntu4) ...
Setting up libc6-dev:arm64 (2.31-0ubuntu9.2) ...
Setting up python3-future (0.18.2-2) ...
update-alternatives: using /usr/bin/python3-futurize to provide /usr/bin/futurize (futurize) in auto mode
update-alternatives: using /usr/bin/python3-pasteurize to provide /usr/bin/pasteurize (pasteurize) in auto mode
Setting up gcc-9 (9.3.0-17ubuntu1~20.04) ...
Setting up openssh-sftp-server (1:8.2p1-4ubuntu0.2) ...
Setting up openssh-server (1:8.2p1-4ubuntu0.2) ...

0 项奖励
回复
97,529 次查看
khang_letruong
Senior Contributor III

I have Ubuntu-18.04 desktop with the packages required by Yocto in the iMX Yocto Project User's Guide :

sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \
build-essential chrpath socat cpio python python3 python3-pip python3-pexpect \
xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \
pylint3 xterm


BR,
Khang

0 项奖励
回复
97,527 次查看
xiaodong_zhang
NXP Employee
NXP Employee

@khang_letruong 

How many DDR Memory?

0 项奖励
回复
97,527 次查看
khang_letruong
Senior Contributor III

@xiaodong_zhang,


My machine has 32GB of RAM :

 

$ free
              total        used        free      shared  buff/cache   available
Mem:       32812796     7672156     1930688      134612    23209952    24551288
Swap:       2097148      804352     1292796

 

Do you have a dockerfile for the generating the building environment btw, please ?

Br,
K

0 项奖励
回复
97,515 次查看
xiaodong_zhang
NXP Employee
NXP Employee

@khang_letruong 

   The issue is caused by package nfs-common (version upgrade after releasing i.MX Yocto ubuntu). You can fix the issue by removing nfs-common in imx-image-desktop.bb.

diff --git a/recipes-fsl/images/imx-image-desktop.bb b/recipes-fsl/images/imx-image-desktop.bb
index ba2f216..1485897 100644
--- a/recipes-fsl/images/imx-image-desktop.bb
+++ b/recipes-fsl/images/imx-image-desktop.bb
@@ -79,7 +79,6 @@ APTGET_EXTRA_PACKAGES += "\
ethtool wget ftp iputils-ping lrzsz \
net-tools \
ntpdate \
- nfs-common \
openssh-server \
python3-future libtool autoconf pkg-config \
bluez connman

97,508 次查看
khang_letruong
Senior Contributor III

Hi @xiaodong_zhang ,

Glad that you found the cause of the issue, I will update the recipe, re-bitbake the image and let you know.

Br,
Khang

 

0 项奖励
回复
97,484 次查看
khang_letruong
Senior Contributor III

Hi @xiaodong_zhang ,

It works great! Thanks very much!

Br,
Khang

0 项奖励
回复
97,773 次查看
刘国华
Contributor III

@xiaodong_zhang 

Hi Xiaodong 

More question :

  1.  Can I.MX8M plus support the ubuntu18.04 or 16.04, as the customer develop many Linux application base on 16.04 , if we can support 16.04 ,it will be better for customer change the platform from Jetson nano to I.MX8m Plus ?
  2. There are some object detection and segmentation samples base on OpenCV in our Yocto RootFS ,but right now our NPU can't support the accelerate compution  .Both the OpenCV and PyTorch inference enginees are currently not supported for running on the NXP NN
    accelerators. Therefore, both frameworks are not included in the above NXP-NN architecture diagram. So if we need using NPU to accelerate compution segmentation and object detection applicaton, how can we do ?
  3. Can our NPU accelerate YoloV4 compution ?
  4. Is there a solution to get the depth data of object thru using 双目 camera? 
0 项奖励
回复
97,761 次查看
xiaodong_zhang
NXP Employee
NXP Employee

Hi @刘国华 

1, Currently i.MX8MP only support to build Ubuntu 20.04 officially. If customer want to build 18.04 or 16.04, please refer to Ubuntu-i.MX8MP.pdf.

2, In OpenCV, only DNN module bases on deep learning. But i.MX8MP NPU don't support DNN. For other machine vision algorithm, OpenCV can be configured to use OpenCL to accelerate. Or choose external vision processor.

3, You can convert TF model of Yolo-v4  to TFlite, and use i.MX8MP NPU as TFlite's backend.

4, China SE team had ported orbbec 3D camera for smart lock, you can get it from marketing Fang Yi.

0 项奖励
回复
94,190 次查看
LamBoo
Contributor I

1. Hi,I'm Build ubuntu20 reference  Ubuntu-i.MX8MP.pdf,but I meet one problem in build

gst-plugins-base
gst-plugins-good
gst-plugins-bad
imx-gst1.0-plugin

In gst-plugins-base when I do

 

# ./autogen.sh --disable-silent-rules --disable-dependency-tracking --disable-gtk-doc --disable-examples --enable-zlib --enable-alsa --disable-cdparanoia --disable-debug --enable-ivorbis --enable-ogg --disable-opus --enable-orc --enable-pango --enable-theora --disable-valgrind --disable-libvisual --enable-vorbis --enable-x --enable-xvideo --enable-xshm --enable-nls --enable-introspection=no --enable-wayland --disable-opengl --prefix=/usr/ CPPFLAGS="-I/usr/include/imx"

It works Error:

LamBoo_0-1656066533630.png

 

but I have Already build and install orc-0.4.27

2. Then I give up install libs above,I copy rootfs to sd card ,It can display weston screen ,when I install xfce and LXDE ,The login page is displayed in a loop.

LamBoo_2-1656066927875.pngI

I look forward to receiving your reply!

标记 (1)
0 项奖励
回复
97,752 次查看
刘国华
Contributor III

@xiaodong_zhang 

In OpenCV, only DNN module bases on deep learning. But i.MX8MP NPU don't support DNN. For other machine vision algorithm, OpenCV can be configured to use OpenCL to accelerate. Or choose external vision processor

So it mearn that we can not accelerate the OpenCV compution using GPU or NPU , it just run on the Cotex-A core (CPU)

0 项奖励
回复
97,803 次查看
xiaodong_zhang
NXP Employee
NXP Employee

hi @刘国华 

1, i.MX8M Plus can support all operator included by tensor flow lite, but not all by NPU. Because if NN API don't support certain operator, TFlite will rollback to CPU. So some models may work without NPU acceleration enabled, and only performance will be impacted.

2, L5.10 can support to build Ubuntu 20.04 image with eIQ and its example, but don't include ROS. Customer need to install ROS by himself. NXP can't release any  Ubuntu  image due to license issue.

3, Jetson Nano has 128 cores GPU with 472GFLOPS, and its performance is 0.92TOPS which is less than half of i.MX8MP.

4,  AI Robot board supports AP1302+AR1335. AR1335+8MP internal ISP is still on-going.

0 项奖励
回复
97,784 次查看
刘国华
Contributor III

@xiaodong_zhang 

AI Robot board supports AP1302+AR1335. AR1335+8MP internal ISP is still on-going.

One more question , how can I get the HW and SW of the camera module board ?

0 项奖励
回复
97,767 次查看
xiaodong_zhang
NXP Employee
NXP Employee

Hi @刘国华 

   You can touch marketing Fang Yi for HW module. SW will be released to you when it's ready.

Add more information:

@刘国华 AR1335 module vendor is AVNET, Contact window is Peterson, Griffin <Griffin.Peterson@AVNET.COM> , onsemi window is Sean Zhang <Sean.Zhang@onsemi.com>

0 项奖励
回复
97,800 次查看
刘国华
Contributor III

@xiaodong_zhang 

Thanks for your reply

Jetson Nano has 128 cores GPU with 472GFLOPS, and its performance is 0.92TOPS which is less than half of i.MX8MP.

How to get the 0.92TOPS base on 128 GPU Jetson nano ? Do you have the computation formula ?

0 项奖励
回复