I.MX8M SD Card Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX8M SD Card Configuration

ソリューションへジャンプ
7,536件の閲覧回数
joshua_eng
Contributor I

Hi, I have a DART-MX8M that is using NXP i.MX8M Evaluation Kit and I have just finished building an image using Yocto with bitbake fsl-image-qt5-validation-imx. I am new to Yocto, but from my understanding I should be able to use the .sdcard image file that is generated in the deploy directory to have a fully ready SD card that I can use for the hardware. I ran the command "sudo dd if=fsl-image-qt5-validation-imx-imx8m-var-dart.sdcard of=/dev/sdb bs=1M && sync" and it created the partition for the root file system on the SD card. It looks like it created the offsets for the U-boot, but to my understanding it should have made the partition after running the command? 

Now after trying to boot the board using the SD card, I set the boot select switch SW7 to the SD side, but when I turn on the board nothing shows up on the screen via the hdmi port. I can tell that it is "running" because I can ping the board to see if packets can be sent/received to it (am unsure if this is a good test). I have never been able to run this board from SD card yet so am unsure if this is normal. Do I have to use putty to run the configuration on the board once it is powered on or should I be expecting something on the screen? 

Other question, do I have to setup each of these partitions manually if using the .sdcard image file does not work?

Another test that I tried running was the SD card recovery image file that was found at ftp://customerv:Variscite[email protected].com/DART-MX8M/Software . I ran the same dd command and tried booting the sd card on the board, but still the same results of nothing appearing on the screen when trying to boot from SD card.

Host environment: Ubuntu Linux 16.04 using VirtualBox.

The SD card is 16GB. 

Any help/advice would be greatly appreciated, and feel free to ask me any questions, I will do my best to supply what you may need from me.

Edit: Some images to provide some more information.

Command ran to setup SD card.

pastedImage_3.png

Partitions for SD card after running dd command:

pastedImage_1.png

File structure of SD card after running command:

pastedImage_4.png

Thanks,

Josh

0 件の賞賛
返信
1 解決策
6,947件の閲覧回数
kaartic_sn
Contributor III

Hi,

Varisicte has separate DTBs for HDMI and LVDS displays. It is possible that by default the DTB used works only with a LVDS display. Try changing the device tree used during boot to the HDMI one using u-boot.

Further, you could try asking help to Variscite's support.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
6,947件の閲覧回数
joshua_eng
Contributor I

Update after spending a day working/researching things. I can boot from my SD card and can run an application via Putty with no errors. The only issue I have now is that I still do not get a display from the hdmi port when booting the sd card and for running the applications. is this a result of missing a package when creating my bitbake images?

There are no compile errors for my Qt5 applications and it appears to be running correctly via Putty. 

Any help would be great!

Thanks,

Josh

0 件の賞賛
返信
6,948件の閲覧回数
kaartic_sn
Contributor III

Hi,

Varisicte has separate DTBs for HDMI and LVDS displays. It is possible that by default the DTB used works only with a LVDS display. Try changing the device tree used during boot to the HDMI one using u-boot.

Further, you could try asking help to Variscite's support.

0 件の賞賛
返信
6,947件の閲覧回数
joshua_eng
Contributor I

Hi, 

That did the trick. Found the correct .dtb file I needed to get my display working. Thanks!

0 件の賞賛
返信