I.MX8 board does not connect to serial using Hyperterminal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX8 board does not connect to serial using Hyperterminal

1,738 Views
ankur_kala
NXP Employee
NXP Employee

Hi,

I have a i.mx 8M Quad evaluation kit and when I try to connect it through USB debug cable as mentioned in the QSG that comes with the board, the system does not recognize the serial ports. As such there is nothing observed over Hyperterm which is set as per the settings mentioned in QSG. The device manager also shows question marks against the ports assigned to the serial term.

Could you please let me know the driver required for the 'enhanced COM port' along with the version number.

Regards,

Ankur

AjeshKumar

Labels (1)
0 Kudos
Reply
1 Reply

1,396 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Use recommendations of "getting started" tab on the EVK page:

i.MX 8M Evaluation Kit|NXP 

Drivers may be loaded from

USB to UART Bridge VCP Drivers | Silicon Labs 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------