Android 7.1.2 MFG-tool image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 7.1.2 MFG-tool image

ソリューションへジャンプ
1,735件の閲覧回数
xiezhiyong
Senior Contributor II

Our product is using imx6qplus and Android 7.1.2.

We want to do eMMC boot.

We use "mfgtoolsL4.9.11_1.0.0" to write eMMC ,but follow  error log is come out.

########################

Wrong Ramdisk Image Format

Ramdisk image is corrupt or invalid

########################

Do the file "fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot" can't be used directly?

How to fix this problem?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,634件の閲覧回数
xiezhiyong
Senior Contributor II

I check config about conig of u-boot .CONFIG_ENV_IS_NOWHERE isn't defined.

I define this config and build u-boot.imx again.

The Ramdisk image can be loaded.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,635件の閲覧回数
xiezhiyong
Senior Contributor II

I check config about conig of u-boot .CONFIG_ENV_IS_NOWHERE isn't defined.

I define this config and build u-boot.imx again.

The Ramdisk image can be loaded.

0 件の賞賛
返信