I.MX7 Flashing Linux using uuu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX7 Flashing Linux using uuu

663件の閲覧回数
mrshafie
Contributor II

hi.

I want to flash linux bsp using uuu on I.MX7 SABRESD board . so I download L4.9.88_2.0.0_images_MX6UL7D.tar.gz from NXP Community. 

for this end I wrote this uuu file:

#=============================================

uuu_version 1.2.39

SDP: boot -f bsp/L4.9.88_2.0.0_images_MX6UL7D/u-boot-imx7dsabresd_sd.imx
FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash -raw2sparse all bsp/fsl-image-validation-imx-xwayland-imx6ul7d.sdcard
FB: flash bootloader bsp/L4.9.88_2.0.0_images_MX6UL7D/u-boot-imx7dsabresd_sd.imx
FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: done

#===============================

I use u-boot-imx7dsabresd_sd.imx and linux image from L4.9.88_2.0.0_images_MX6UL7D.tar.gz package. but this is output:

#============== output

.

.

Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args; if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else bootz ${loadaddr} ${initrd_a;
Hit any key to stop autoboot: 0
Bad Linux ARM zImage magic!

#===========

can any body help me? how to flash linux on i.mx7d using uuu? 

Thanks for your attention.

0 件の賞賛
返信
0 返答(返信)