Busfreq OPTEE set from 24000000 to 400000000 start.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Busfreq OPTEE set from 24000000 to 400000000 start.

Jump to solution
1,914 Views
layleon
Contributor III

There is a lot of this information that will always be displayed periodically, why? How to mute it? Can I only modify the source code without printk? 

[  206.247131] Busfreq OPTEE set from 400000000 to 24000000 start...
[  206.255946] Busfreq OPTEE set to 24000000 done! cpu=0
[  206.295989]
[  206.295989] Busfreq OPTEE set from 24000000 to 400000000 start...
[  206.332122] Busfreq OPTEE set to 400000000 done! cpu=0
[  209.447133]
[  209.447133] Busfreq OPTEE set from 400000000 to 24000000 start...
[  209.455924] Busfreq OPTEE set to 24000000 done! cpu=0
[  209.496017]
[  209.496017] Busfreq OPTEE set from 24000000 to 400000000 start...
[  209.532123] Busfreq OPTEE set to 400000000 done! cpu=0
[  212.647100]
[  212.647100] Busfreq OPTEE set from 400000000 to 24000000 start...
[  212.655921] Busfreq OPTEE set to 24000000 done! cpu=0
[  212.696172]
[  212.696172] Busfreq OPTEE set from 24000000 to 400000000 start...
[  212.732340] Busfreq OPTEE set to 400000000 done! cpu=0
[  215.847153]
[  215.847153] Busfreq OPTEE set from 400000000 to 24000000 start...
[  215.855952] Busfreq OPTEE set to 24000000 done! cpu=0
[  215.895905]
[  215.895905] Busfreq OPTEE set from 24000000 to 400000000 start...
[  215.931981] Busfreq OPTEE set to 400000000 done! cpu=0
[  219.047116]
[  219.047116] Busfreq OPTEE set from 400000000 to 24000000 start...
[  219.055954] Busfreq OPTEE set to 24000000 done! cpu=0
[  219.115985]
[  219.115985] Busfreq OPTEE set from 24000000 to 400000000 start...
[  219.141949] Busfreq OPTEE set to 400000000 done! cpu=0
[  222.727073]
[  222.727073] Busfreq OPTEE set from 400000000 to 24000000 start...
[  222.735873] Busfreq OPTEE set to 24000000 done! cpu=0
[  222.775976]
[  222.775976] Busfreq OPTEE set from 24000000 to 400000000 start...
[  222.812075] Busfreq OPTEE set to 400000000 done! cpu=0
[  225.927155]
[  225.927155] Busfreq OPTEE set from 400000000 to 24000000 start...
[  225.935970] Busfreq OPTEE set to 24000000 done! cpu=0
[  225.975879]
[  225.975879] Busfreq OPTEE set from 24000000 to 400000000 start...
[  226.012141] Busfreq OPTEE set to 400000000 done! cpu=0
[  229.127121]
[  229.127121] Busfreq OPTEE set from 400000000 to 24000000 start...
[  229.135966] Busfreq OPTEE set to 24000000 done! cpu=0
[  229.176856]
[  229.176856] Busfreq OPTEE set from 24000000 to 400000000 start...
[  229.212407] Busfreq OPTEE set to 400000000 done! cpu=0
[  232.487115]
[  232.487115] Busfreq OPTEE set from 400000000 to 24000000 start...
[  232.495906] Busfreq OPTEE set to 24000000 done! cpu=0
[  232.536256]
[  232.536256] Busfreq OPTEE set from 24000000 to 400000000 start...
[  232.571992] Busfreq OPTEE set to 400000000 done! cpu=0
[  235.687101]
[  235.687101] Busfreq OPTEE set from 400000000 to 24000000 start...
[  235.695880] Busfreq OPTEE set to 24000000 done! cpu=0
[  235.754748]
[  235.754748] Busfreq OPTEE set from 24000000 to 400000000 start...
[  235.781876] Busfreq OPTEE set to 400000000 done! cpu=0

 

0 Kudos
Reply
1 Solution
1,869 Views
igorpadykov
NXP Employee
NXP Employee

one can look at sect.2.5.4 Dynamic Bus Frequency  i.MX Linux Reference Manual​

so if voltages are fixed, busfreq driver may be disabled. Depending on processor load voltages may

vary as "fsl,soc-operating-points" show in dts

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ull.dtsi?h=imx_5.4.4...

 

Best regards
igor

View solution in original post

0 Kudos
Reply
6 Replies
1,900 Views
igorpadykov
NXP Employee
NXP Employee

Hi layleon

 

what processor and bsp used in the case. Is it possible to reproduce issue on some nxp

reference board with demo images from:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos
Reply
1,897 Views
layleon
Contributor III

BSP:5.4.47_2.2.0​​

Self-designed hardware, using IMX6UL.

Boot from NAND.

微信截图_20201210174408.png

0 Kudos
Reply
1,882 Views
igorpadykov
NXP Employee
NXP Employee

"Self-designed hardware" - uses pmic or based on nxp i.MX6UL EVK reference design ?

 

Best regards
igor

0 Kudos
Reply
1,878 Views
layleon
Contributor III

fixed 3V3/1V2/1V35 by DC-DC converter

The same DDR P/N, 128MB NAND, has been booted and the DDR has been calibrated.

Reading the code, it looks like the DDR frequency keeps changing(periodicity) from 24MHz to 400MHz(400MHz to 24MHz), which triggers this change, why is this? This output is very disturbing to debug ah.

 

微信截图_20201210220008.png

 

微信截图_20201210215903.png

0 Kudos
Reply
1,870 Views
igorpadykov
NXP Employee
NXP Employee

one can look at sect.2.5.4 Dynamic Bus Frequency  i.MX Linux Reference Manual​

so if voltages are fixed, busfreq driver may be disabled. Depending on processor load voltages may

vary as "fsl,soc-operating-points" show in dts

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ull.dtsi?h=imx_5.4.4...

 

Best regards
igor

0 Kudos
Reply
1,859 Views
layleon
Contributor III

Example Patch,both the kernel(linux-imx) and the bootloder(u-boot) need to be patched.

 

diff --git a/arch/arm/boot/dts/imx6ul.dtsi b/arch/arm/boot/dts/imx6ul.dtsi
index 3a9985cb0dd9..e0809eabf4ff 100644
--- a/arch/arm/boot/dts/imx6ul.dtsi
+++ b/arch/arm/boot/dts/imx6ul.dtsi
@@ -59,22 +59,16 @@
 			compatible = "arm,cortex-a7";
 			device_type = "cpu";
 			reg = <0>;
-			clock-frequency = <696000000>;
+			clock-frequency = <528000000>;
 			clock-latency = <61036>; /* two CLK32 periods */
 			#cooling-cells = <2>;
 			operating-points = <
 				/* kHz	uV */
-				696000	1275000
 				528000	1175000
-				396000	1025000
-				198000	950000
 			>;
 			fsl,soc-operating-points = <
 				/* KHz	uV */
-				696000	1275000
 				528000	1175000
-				396000	1175000
-				198000	1175000
 			>;
 			clocks = <&clks IMX6UL_CLK_ARM>,
 				 <&clks IMX6UL_CLK_PLL2_BUS>,

 

0 Kudos
Reply