I.MX6Solo video input signal synchronized checking register.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I.MX6Solo video input signal synchronized checking register.

跳至解决方案
1,466 次查看
takashitakahash
Contributor III

Dear community.

Our customer has question below.

I would like to tell you about Video input of iMX6,
Is there a way to check if the video input is synchronized with register values?

I am planning to detect it when the screen scrolls when the input signal is unstable.

Thank you,

Best Regards.

T.Takahashi.

标签 (1)
0 项奖励
回复
1 解答
1,365 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takahashi

I am afraid there are no such ipu register bits which would indicate

loss of synchronization, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,366 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takahashi

I am afraid there are no such ipu register bits which would indicate

loss of synchronization, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复