I.MX6Solo video input signal synchronized checking register.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6Solo video input signal synchronized checking register.

ソリューションへジャンプ
1,531件の閲覧回数
takashitakahash
Contributor III

Dear community.

Our customer has question below.

I would like to tell you about Video input of iMX6,
Is there a way to check if the video input is synchronized with register values?

I am planning to detect it when the screen scrolls when the input signal is unstable.

Thank you,

Best Regards.

T.Takahashi.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,430件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takahashi

I am afraid there are no such ipu register bits which would indicate

loss of synchronization, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,431件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takahashi

I am afraid there are no such ipu register bits which would indicate

loss of synchronization, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信