I.MX6Solo video input signal synchronized checking register.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Solo video input signal synchronized checking register.

Jump to solution
1,468 Views
takashitakahash
Contributor III

Dear community.

Our customer has question below.

I would like to tell you about Video input of iMX6,
Is there a way to check if the video input is synchronized with register values?

I am planning to detect it when the screen scrolls when the input signal is unstable.

Thank you,

Best Regards.

T.Takahashi.

Labels (1)
0 Kudos
Reply
1 Solution
1,367 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takahashi

I am afraid there are no such ipu register bits which would indicate

loss of synchronization, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,368 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takahashi

I am afraid there are no such ipu register bits which would indicate

loss of synchronization, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply